This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how do we connect ads 1298 front end to pc

Other Parts Discussed in Thread: ADS1298, ADS1298ECGFE-PDK

Dear friends,

                      how do we connect ads1298 front end to pc. is the front end module have a usb. please help me in this regard

Thank you

 

  • Hello Dushyanth,

    The ADS1298 would need to be connected to some sort of host controller. There is no built in USB or RS-232 type communication scheme with the ADS1298 itself. Our evaluation platform for the ADS1298, which is the ADS1298ECGFE-PDK, uses a TMS320VC5509 DSP. This is then connected to the PC, via USB cord (standard USB-type B to type A).

    Regards,

    Michael