Other Parts Discussed in Thread: ADS54J20EVM
Hello
I would like to use the following ADC, DAC & capture EVMs for our experimental setup
TSW14J56 -> ADS54J20EVM (dual channel, 12bit, 1GSPS ADC)
TSW1406 -> DAC5682ZEVM (dual channel, 16bit, 1GSPS DAC)
I wanted to confirm that our requirements can be met with this
1) I need the ADC and DAC sampling to be synchronized. What is the best way to do this and what kind of timing precision can we expect ex, within 100ps? Do we need the TSW1400 for this or will the TSW1406 work?
2) We want to play out a signal pattern from the DAC that is say 50us long and simultaneously capture ADC samples
3) We want to repeat this multiple times with say 10us gap ie, play out the signal every 60us
4) We would like to generate a trigger signal every time this process starts ie, every 60us?
5) We would like this process to repeat till the TSW14J56 memory fills up at which point the DAC and trigger signals stop as well.
6) Do you have suggestions on how to minimize the data transfer time to a PC. What kind of throughput can we expect from the "TSW14J56 -> PC" over USB3.0. A rough guidance would help.
7) An alternative for us might be to use "TSW14J56 -> DAC3XJ8XEVM (dual channel, 16bit, 1.6GSPS DAC)" instead of the above TSW1406/DAC5682ZEVM combination if it makes things easier/more precise
Thank you.