Part Number: AFE4300
Dear Sir,
We are using AFE4300 along with STM32L031. We want to measure weight using AFE4300. For this according to the datasheet one of the terminals of a load cell should be connected to the VLDO pin which will drive the load cell circuit. For getting this voltage as suggested in the datasheet i tried to set the power -on bit in device_control_register and switch on weight chain. But the board doesn't seem to be responding appropriately. If I write the prescribed value onto the register and read it ,it seems to reflect a value of its own and not the value i have written. Any suggestions or help will be appreciated.
Regards,
Muthu S