Part Number: DDC112
Hello everyone:
I use stm32F1 to drive the DDC112, I get the 12Mhz CLK for DDC112 based on stm32F1 PWM output. And also get the CONV based on stm32F1 another PWM out (50% duty). When I set the CONV time is 1000ms,the it should work as continue mode, No signal is connect to DDC112,I get the below result using stm32 mcu SPI function:
ch1:-36.05 ch2:-46.49fA
ch1:-58.68 ch2:-48.85fA
ch1:-35.48 ch2:-45.22fA
ch1:-59.11 ch2:-48.99fA
ch1:-34.12 ch2:-44.33fA
ch1:-56.33 ch2:-50.54fA
ch1:-34.87 ch2:-47.53fA
ch1:-58.35 ch2:-49.18fA
ch1:-36.05 ch2:-46.64fA
ch1:-58.64 ch2:-50.68fA
ch1:-34.12 ch2:-45.84fA
ch1:-57.60 ch2:-49.55fA
ch1:-36.09 ch2:-49.22fA
We can see the CH1 result has stage,-36->-58->-34,I do not konw why. And CH2 seemed only a little.
When I set the CONV time is 50ms integrating time,also no input to DDC112, data is below:
ch1:-470.59 ch2:-367.06fA
ch1:-477.18 ch2:-424.47fA
ch1:174.12 ch2:89.41fA
ch1:169.41 ch2:106.35fA
ch1:164.71 ch2:93.18fA
ch1:134.59 ch2:41.41fA
ch1:-442.35 ch2:-312.47fA
ch1:-419.77 ch2:-249.41fA
ch1:-378.35 ch2:-174.12fA
ch1:30.12 ch2:-236.24fA
ch1:2.82 ch2:-297.41fA
ch1:-15.06 ch2:-358.59fA
ch1:-291.76 ch2:64.00fA
ch1:-278.59 ch2:64.00fA
ch1:-265.41 ch2:38.59fA
ch1:-306.82 ch2:-1.88fA
ch1:9.41 ch2:-293.65fA
ch1:40.47 ch2:-228.71fA
ch1:79.06 ch2:-140.24fA
ch1:-432.00 ch2:-299.29fA
ch1:-467.77 ch2:-370.82fA
ch1:-475.29 ch2:-437.65fA
ch1:-489.41 ch2:-434.82fA
ch1:176.00 ch2:83.76fA
We can see there is big fluction, can you help me?