This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7142: ADS7142 I2C BUS

Part Number: ADS7142

Hi,

Will the ADS7142 load the I2C Bus when it is powered off?  (AVDD , DVDD = 0)

  • Hi David

    When AVDD and DVDD is 0V (Device is powered off), the SCL/SDA output FET will see a floating voltage at the gate and respective pin loading can not be determined.

    We recommend to keep device powered on when connected to I2C bus / other active devices connected on the same bus.

    Thanks & Regards
    Abhijeet