Part Number: ADS1232
Hi,
For a weighing scale project I want to use ADS1232 ADC. I The sensitivity of load cell is 2mV/V +-0.2V. The load cell capacity is 120Kg and resolution required is 30000. As per my calculation the load cell will output 333nV/gram. Now the question is can I use ADS1232 for our application.
With ADS1232 can we read the data every 400ms?
Thanks,
Sreekanth