Part Number: DDC11XEVM-PDK
Other Parts Discussed in Thread: DDC112
The DDC11xEVM-PDK Kit Operation guide states the following:
"HARDWARE TRIGGER: In normal operation, this should be Disabled. If Enabled, a pulse can be issued on IP_1 to start a conversion after Take Data is pressed."
This is the only reference in the document to the hardware trigger, or to IP_1. I need to use the hardware trigger to synchronize acquisition on the DDC112 to my source. Can you please tell me where IP_1 is on the EVM?
Thank you,
-phil