Hello,
I have a four layer PCB on which I placed a two-layer PCB coil design on the top two layers. It needs to measure the distance to a piece of metal above the pcb, anything below the coil should not have any impact on it.
My problem is that I need to route a trace on the fourth (bottom) layer under the PCB coil. Obviously, this is giving me a lot of noise on the measured inductance. Could I do something like a ground plane on the third layer to remove this noise? Could I make use of chapter 2.1.2 from the document below, or is this meant for other situations? Are there other things I could take into consideration for the design to make this work?
The document: http://www.ti.com/lit/an/snoa962/snoa962.pdf
I look forward to hearing from you!