Hello,
I am currently interfacing the ADS8832 and am wondering how to best go about it.
In "9.5.4 Reading the Conversion Result" the datasheet states "The conversion result is available to the input of the output data register (ODR) at EOC and presented to the output of the output register at the next falling edge of FS/!CS.The host processor can then shift the data out through the SDO pin at any time except during the quiet zone. This duration is 20 ns before and 20 ns after the end of sampling (EOS) period."
Does this mean, that it is mandatory to sync the SPI transfer to the EOC? What happens if a SPI transfer is timed so that it collides with the quiet zone?
With kind regard