Part Number: ADC12D1800RFRB
Dear all,
I am working with the reference board ADC12D1800RF (the one who has the FMC expansion connector) and I have the problem that the I and Q channels are not synchronized as viewed in the Wave Vision software, i.e., there is a time offset between the channels despite the fact that the inputs to both channels are the same. I am using the FPGA source code obtained from the ADC's TI web, to create the bit file. The problem is solved if I use the bit file that I found in the forum (adc10d1000_xc4vlx25_adc12d1600rfrb.bit). Please, could you provide me the source code that was used for generate this bit file? Thanks,
Juan