Part Number: ADS8329
Hi Team,
In my customer's application, the input signal is range from the 0~3V, and they need to make sure the16 bit resolution when the sample rate is 1MHz. And the supply voltage is about 3.3V to 5V.
I have recommended the ADS8329
So I want to know any factor I need to consider to meet the requirement I have described above?
Thanks a lot!
Lacey