Dear Folks
According to the datasheet of ULN2003ANSR, it mentions the relative between duty cycle and output current on figure 4. But it doesn't refer and contain the restriction of the period such as whole period doesn't exceed 10ms something like that...
Is there any possibility that relay operation time is larger than ULN2003ANSR's operation time? If do so. Does it make unexpected condition?