This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300: Pls. Verify

Part Number: AFE4300

Hello,

I am using AFE4300 with STM32L0. I have programmed the spi to write 0x6005 to the 0x09 (device control register) register and 0x4140 to the 0x01(adc control register) register in order to power on the afe and the weight chain (to obtain 1.7V on the VLDO pin). Can you please verify if this is correct? Also if any wrong values are written will it be fine if i reset the AFE or is there possibility of damage because of wrong writes.

Thanks and Regards

Abhinav