Part Number: ADS8685
hi,
Does ADS8685 require an external Input protection circuit? This question is because of the fact that it already has a OVP inside of it.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS8685
hi,
Does ADS8685 require an external Input protection circuit? This question is because of the fact that it already has a OVP inside of it.
Hello VEERAMANI,
Welcome to E2E forum.
ADS8685 has internal input protection circuit and it can provide a protection up to +/-20V(+/-11V for loss of AVDD), but if an overvoltage on the input is a common event in your system, external diodes are strongly recommended to use on the input of the ADC as a secondary clamp protection, also a resistor is recommended in series with the input to limit the current and protect ADC input and the diodes.
Thanks
Best®ards
Dale