Part Number: FDC2114EVM
Other Parts Discussed in Thread: FDC2114
I am trying to plot the change in capacitance using the FDC2114EVM, and the FDC2114EVM GUI, and log this data to an excel file. I purchased this boards because the datasheet says that it can achieve a maximum output rate of 13ksps.
According to the graph configuration tab, the Data Sample Rate can only achieve around 400 sps. Adding samples to the graph at faster rate plots the same data samples more than once, instead of sampling at a faster rate.
I have altered the reference and sample count on the configuration tab, however the data still can only achieve 400 sps, regardless of how I change these two values.
How can I achieve a faster sampling rate?