Part Number: ADC12DS080
Other Parts Discussed in Thread: ADC12DS105
Hi all, and thanks in advance for your responses.
I'm designing a board that uses this particular IC to measure some fully differential signals. What kind of circuit should I use at the input to drive the ADC properly? The input circuitry suggested in the datasheet is made up of baluns to transform common mode signals to fully differential and so is of no use to me.
Also, I will probably be oversampling the signals and using as much as I can get of this part's full scale bandwidth (which is 1GHz), so I have to take this into account. I've been doing some reading on various application notes on using ADC drivers, but am not sure what (if anything), I need. I've seen this part used succesfully right on the ouput of an IQ Demodulator (LTC5586) with only an antialias filter in between, but since I will be measuring different signals off of different boards, I'm unsure as to what I have to take into account.
Again, thanks for your responses, any and all help you can give me on the matter is much appreciated.