Other Parts Discussed in Thread: ADS1248,
Customer Question:
1. On the ADS1248 when used in unipolar mode the negative reference output should be tied to AVSS and in bipolar mode states that the negative reference output should be tied to the midpoint between AVDD and AVSS. For the ADS124S08, the datasheet claims that the reference output should be tied to AVSS always.
I can’t quite wrap my head around how I would use the ADS124S08 reference output in bipolar mode. I want to use the internal reference buffered and amplified to power the strain gauge excite voltage, which is 2.5V referenced to AGND, but if the reference output negative is tied to the negative supply, what is the positive reference output level be with respect to the midpoint of AVDD and AVSS?, In my design AVDD is +2.5V and AVSS is -2.5V. If the reference is also 2.5V and is referenced to -2.5V, is VREFOUT sitting at 0V (AGND)?
2. A further question somewhat related is whether there is any harm in using bipolar supplies when measuring a unipolar input? I also want to read a single ended voltage input that has AGND as the reference input. I did this with the ADS1248, but the change in the reference connections has me concerned.