Hi,
I have design a board around the ADS1278. I have copied down some EVM board parts to be sure that my tracks, my plans (ground and power) and my components (capacitors, reference voltage...) are good. My configuration is "Hight precision" and my clock is 20MHz (frequency modulator at 5MHz). I use single ended inputs without differential amplifier. I have put all the AINN to VREF, but because my results was too bad, I put them now to AGND (my AINP input ranges is 2.5V now).
When I put an AINP to AGND, the AINP is clean (my noise is below 5mv, without specific frequency). The Code peak-to-peak for 20 measures has an average below 200. I have bought an EVM board to compare my results. I have modified the EVM Channel 1 to be in the same conditions : AINN to AGND and I removed the 2 resistors at the input of the amplifier (R17, R18). I added a 33k resistor in parallel of the C0G capacitor (C20) because the amplifier (U11) adds an impedance on the other channels that improve the results (i think). I put this resistor on my board too. The Code p-p for 20 mesures of AGND has an average of 100 with the EVM board.
When I put a battery of 1.2V to an AIPN of my board, this AINP input gets voltage peaks of 30mv at 5MHz (frequency modulator). With the EVM board, I haven't got these peaks if i connect the battery to the screws, but i have 10mv peak to peak on AINP if I connect the battery on the C0G input capacitor (C20) (this configuration is close to my board). I have disconnected all the AINN from the ground of my board, exepted the Channel 1 (I think the modulator operates over all the channels in the same time, so a surge current is possible), but the voltage peaks persist. With the battery as input, the Code peak-to-peak of my board is 8000, the EVM Code p-p is 105 if connected to the screw, 230 if connected to C20.
There has to be an explanation of the presence of the frequency modulator peak at the AINP input... Someone has an idea ? Help is welcome !
Thanks.
PS : I join screenshots of my oscilloscope. The probe is between AGND and the positive contact of the battery (1.2V).