Other Parts Discussed in Thread: ADS8668
HI Sir
I link the ADS8668 with NB, Show as below, may I lost any thing?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
When you plug in the USB cable, the GUI will talk to SDCC also the GUI/SDCC will verify the information saved in the SD card on the bottom side of EVM. I just tried to connect SDCC only to the laptop, I got same error information as you which was reported by the GUI, so suggest you to connect both EVM and SDCC together, then plug into the USB port.
Thanks®ards
Dale
Hi Alex,
To connect the EVM to laptop with the GUI, the external 5-V DC power supply on J32 is not needed, this external power supply is only used to generate high voltage supplies(HVDD and HVSS) for buffers U4 and U5 on RVM board.
Just confirm: Are you using ADS86xxEVM with SDCC? Are you using ADS86XX EVM GUI downloaded from TI.com? Is the OS on your laptop Win 10?
Thanks.
Best regards
Dale
Hi Alex,
Can you please clarify what the error or failure is? by the way, I have shared a update driver with you, please check, thanks.
Best Regards
Dale