Hello TI Team,
We are currently using an ADS1299 to acquire 8 channel data as in ADS1299EEGFE-PDK board.
To begin with, we referred to the datasheet for ADS1299 & ADS1299EEGFE-PDK board and made connections to each pin as per requirement. Further, when we supplied the ADS1299 with 5V and GND (Unipolar) as power supplies, it got heated up quickly. To troubleshoot it, we proceeded with probe testing the connections made but all the connections were connected correctly and the voltages read were to the right values.
As an alternative, we provided the ADS1299 with 2.5V and -2.5V (Bipolar) supplies and as a result, we observed no heating up issue of the IC. We then proceeded further to tested our board for SPI communications (that worked perfectly for ADS1299FE Board as we were able to read a channel’s data correctly) and observed that the values of registers were read correctly but the data being received was intermittent.
Can you please let us know the possible reasons for the same?
Thanks!
P.S - Providing Bipolar supplies, the SPI clock signal was probed to compare with its ideal waveform: SPI Clock was similar to as seen from ADS1299FE Board.