Other Parts Discussed in Thread: LMR14203, INA826, ADS1220, ADS1231, ADS1232, ADS124S06, ATL431LI
Hello,
I am designing a system to measure for load cells with the following characteristics:
- Sensitivity of 2mV/V
- Accuracy class of 3000
- Input Voltage of 10V
- Max load 20kg
- Min load 10gr
- Only Force in one direction is measured
The system is power with 24V. I am using two LMR14203: One for the Analog circuit (10V) and other for the Digital Circuit (5V).
So far I am using INA826 in my simulations to amplify the load cell voltage and everything works nice.
My concern is about the ADC conversion. I was thinking in an ADC with 20bit with ratiometric measurement, but I don't find any ADC with
an Analog Input Ref Voltage of 10V. What do you think about everything? Is there and ADC with 10V analog ref?
Can I use ratiometric measurement in some way with an ADC with 5V analog ref?
Thank you so much for your help!