This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP7002 1.9V verses TVP70025 1.8V

Other Parts Discussed in Thread: TVP7002

Per datasheet the TVP7002 wants 1.9V for its core voltage verses the TVP70025 which specifies 1.8V. I know the 70025 is specified for industrial temperatures and cost more. The TVP7002 can digitize at higher frequencies. The questiosn is: Can the TVP7002 be operated with a 1.8V core voltage? I suspect doing so, will limit the frequency to something similar or the same as the TVP70025. True?

I only need the performance of the TVP70025 at comercial temperatures. I do not have any other devices requiring 1.9V. I already have 1.8V onboard. Also, prefer the cost of the TVP7002. Plus, the TVP7002 appears to be more readily avaible from distribution. Recommendations?

Thanks