Part Number: ADC34J45EVM
Other Parts Discussed in Thread: LMK04828
Hi,
I am using ADC34j45EVM. I follow the steps in the user guide:
1. The evaluation of the ADC32J/34Jxx EVM requires programming the LMK04828 clock source with the
correct PLL settings to provide a 160 Msps clock.
• Connect a USB cable from the ADC32J/34Jxx EVM to the PC
• Open the ADC3000 GUI, and connect to the ADC32Jxx or ADC34Jxx EVM
• Go to the Low Level tab and click Load Config
• Browse and find the ADC3xJxx_160MSPS_Operation_LMK_Setting.cfg
• Check that the PLL2 LED D4 is lit – this indicates that the PLL is programmed properly and the
correct clocks are being generated
But I did not find the "ADC3xJxx_160MSPS_Operation_LMK_Setting.cfg" . The PLL2 LED D4 is not lit.
Can anyone tell me why and what to do?
Thanks a lot.