This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970: Configurable range of demodulator BPF bandwidth

Part Number: PGA970


Hello, 

I think that PGA970 is not intent to measurement for over 500Hz frequency LVDT core movement.

Is it right ?

Why I came to think of that way is because configurable range of demodulator BPF bandwidth is up to 1 kHz.

Refer to [1], Ideally It is expected to extract only Frequency range ωc ± ωs using BPF.  

So I think actually the  ωs range is  restricted to under 500Hz. 

[1] “Dealing with nonlinearity in LVDT
position sensors,” Texas Instruments Analog
Applications Journal (SLYT582),