This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2114EVM: Issue with proximity detection

Part Number: FDC2114EVM
Other Parts Discussed in Thread: FDC2114, FDC2214, LDC2114, , FDC2214EVM

I recently received the FDC2114 Evaluation module and after testing it we are only getting significant changes in the capacitance when the plate is directly touched. For our application we would like to be able to have a bigger change in the capacitance when an object comes within approximately 2cm to 4cm range of the sensor (but not directly touching), after playing with the evaluation board we are only getting about a change in the capacitance of about 0.4pF. What should we do in order to increase the resolution of the changes in the capacitance in the 2cm to 4cm range?