Part Number: AFE4490
Other Parts Discussed in Thread: MSP430F5529
In SPI Interface, MOSI is working but MISO is not working. I also tried writing to a register (which is R/W) and reading the same via SPI interface. SPI write operation works successfully but at the same time, SPI read does not work. Through the code i tried these steps to check working of MISO:
1. Disable SPI_READ of CONTROL0.
2. Enable SW_RST, DIAG_EN
3. Enable SPI_READ
4. Read DIAG register (address: 0x30)
5. Disable SPI_READ
But i could not read DIAG register. Please someone help me with this.