Part Number: ADS1292
Dear TI,
I'm using ADS1292 for measuring current through current sense resistor. AVDD is connected to +3.3V. AVSS is connected to 0V (GND). VREFP = +2.5V. VREFN = 0V (GND).
IN1P - 0,916V (Voltage across sense resistor), IN1N - 0,416V (Voltage divider from reference 2.5V/6). I want to measure difference voltage 0,916V - 0,416V = 0,5V (about 1700000 AD units).
I want to turn on PGA with amplification of 4. Difference voltage 0,5 * 4xPGA = 2V output = 6800000 AD units, less than 8388608. I always get something about 4200000 AD units (about 1.25V - 2.5V refenence / 2).
From ADS1292 data sheet, equation (7) I saw that max input voltage INP-INN < Vref / Gain. So from my example, 2V is 0.5V less than Vref.
Also from Table 10. it can be seen that full scale 0x7FFFFF = Vref (2.5V from my example) and 0x800000 = -Vref (0V from my example).
Can you please tell me where is problem with my AD units result, and why i cannot get 6800000 instead of 4200000?
Best regards,
Vojin Ilic