This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DL3200: LVDS Synchronization

Part Number: ADC12DL3200


Hi, I would need a specific information on the Synchronization behaviour of the component. The question is simple and direct, I am developing the FPGA firmware to manage the ADC LVDS data signals,

does the activation of  SYSREF signal reset the DACLK/DBCLK.. signals? or reset only the demultiplexing of the data?

  • Hi Gianpiero
    The applied SYSREF signal sets or re-aligns the timing of the de-multiplexed output Dx data signals, DxSTRB strobe signals and the DACLK/DBCLK/DCCLK/DDCLK/ output clocks.
    If a new SYSREF event is performed which does not change the existing timing (because SYSREF is frequency and phase locked to CLK and is at the proper frequency and setup/hold time), those signals would not be affected.
    Let me know if you need any additional information.
    Best regards,
    Jim B
  • Hi Jim,

    thank you for the ready answer, just to be sure that I have understood well, at the first activation of the SYSREF signal I should expect a re-aligning of the DACLK/DBCLK/DCCLK/DDCLK/ output clocks (that means a discontinuity of them, shorter/longer cycles) and after, if the SYSREF frequency and phase lock is correct the DACLK/DBCLK/DCCLK/DDCLK/ output clocks should not more impacted by the SYSREF activation. Correct?
  • Hi Gianpiero
    That is correct.
    Best regards,
    Jim B