Part Number: ADS1263
Other Parts Discussed in Thread: ADS1262
as suggest by Chris, I go ahead but nothing get resolved. Issue is still there basic problem from my point of view when I see the example given by TI
- How to configure that which ADC get initialized and where to read its data as ADC had 11 channels no. in it
- no timing diagram is provided in data sheet (this definitely give easy way to us to know its working)
- i had done some initialization and as below but don't know where the issue is
////////////////////////// INCLUDE FILE ////////////////////////////////////////
#include "ADS1263.h"
////////////////////////// PIN DECLARATIONS ////////////////////////////////////
sbit defADC1263_RESETPin at GPIOE_ODR.B2;
sbit defADC1263_STARTPin at GPIOE_ODR.B3;
sbit defADC1263_CSPin at GPIOE_ODR.B4;
sbit defADC1263_DRDYPin at GPIOE_ODR.B5;
sbit defADC1263_SCKPin at GPIOB_ODR.B3; //
sbit defADC1263_DOUTPin at GPIOB_ODR.B4; //
sbit defADC1263_DINPin at GPIOB_ODR.B5; //
char j;
/*
ADS1262.h - Library for ADS1262 Shield Arduino Firmwar.
Created by Protocentral, December 27, 2013.
Released into the public domain.
*/
char* ads1262_Read_Data(){
static char SPI_Dummy_Buff[6];
defADC1263_CSPin_Clr;
for (j = 0; j < 6; ++j){
SPI_Dummy_Buff[j] = SPI3_Read (CONFIG_SPI_MASTER_DUMMY);
}
defADC1263_CSPin_Set;
return SPI_Dummy_Buff;
}
void ads1262_Init(){
GPIO_Digital_Output(&GPIOB_BASE, _GPIO_PINMASK_3 | _GPIO_PINMASK_5);
GPIO_Digital_Output(&GPIOE_BASE, _GPIO_PINMASK_2 | _GPIO_PINMASK_3 | _GPIO_PINMASK_4);
GPIO_Digital_Input (&GPIOE_BASE, _GPIO_PINMASK_5);
GPIO_Digital_Input (&GPIOB_BASE, _GPIO_PINMASK_4);
//defADC1263_RESETPin_Set;
//defADC1263_STARTPin_Set;
//defADC1263_CSPin_Set;
//defADC1263_SCKPin_Set;
//defADC1263_DINPin_Set;
//while(1);
// start the SPI library:
// SPI.begin();
// SPI.setBitOrder(MSBFIRST);
//CPOL = 0, CPHA = 1
// SPI.setDataMode(SPI_MODE1);
// Selecting 1Mhz clock for SPI
// SPI.setClockDivider(SPI_CLOCK_DIV8); // DIV16
// hs
// SPI2_Init();
SPI3_Init();
ads1262_Reset();
Delay_ms(100);
// ads1262_Disable_Start();
// ads1262_Enable_Start();
ads1262_Hard_Stop();
// ads1262_Start_Data_Conv_Command();
// ads1262_Soft_Stop();
Delay_ms(50);
// ads1262_Stop_Read_Data_Continuous(); // SDATAC command
Delay_ms(300);
ads1262_Reg_Write(POWER, 0x11); //Set sampling rate to 125 SPS
Delay_ms(10);
ads1262_Reg_Write(INTERFACE, 0x05); //Lead-off comp off, test signal disabled
Delay_ms(10);
ads1262_Reg_Write(MODE0, 0x00); //Lead-off defaults
Delay_ms(10);
ads1262_Reg_Write(MODE1, 0x80); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(MODE2, 0x06); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(INPMUX, 0x01); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(OFCAL0, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(OFCAL1, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(OFCAL2, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(FSCAL0, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(FSCAL1, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(FSCAL2, 0x40); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(IDACMUX, 0xBB); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(IDACMAG, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(REFMUX, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(TDACP, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(TDACN, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(GPIOCON, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(GPIODIR, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(GPIODAT, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(ADC2CFG, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(ADC2MUX, 0x01); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(ADC2OFC0, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(ADC2OFC1, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(ADC2FSC0, 0x00); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Reg_Write(ADC2FSC1, 0x40); //Ch 1 enabled, gain 6, connected to electrode in
Delay_ms(10);
ads1262_Start_Read_Data_Continuous();
Delay_ms(10);
ads1262_Enable_Start();
}
void ads1262_Reset(){
defADC1263_RESETPin_Set;
Delay_ms(100); // Wait 100 mSec
defADC1263_RESETPin_Clr;
Delay_ms(100);
defADC1263_RESETPin_Set;
Delay_ms(100);
}
void ads1262_Disable_Start(){
defADC1263_STARTPin_Clr;
Delay_ms(20);
}
void ads1262_Enable_Start(){
defADC1263_STARTPin_Set;
Delay_ms(20);
}
void ads1262_Hard_Stop (void){
defADC1263_STARTPin_Clr;
Delay_ms(100);
}
void ads1262_Start_Data_Conv_Command (void){
ads1262_SPI_Command_Data(START); // Send 0x08 to the ADS1x9x
}
void ads1262_Soft_Stop (void){
ads1262_SPI_Command_Data(STOP); // Send 0x0A to the ADS1x9x
}
void ads1262_Start_Read_Data_Continuous (void){
ads1262_SPI_Command_Data(RDATAC); // Send 0x10 to the ADS1x9x
}
void ads1262_Stop_Read_Data_Continuous (void){
ads1262_SPI_Command_Data(SDATAC); // Send 0x11 to the ADS1x9x
}
void ads1262_SPI_Command_Data(unsigned char data_in){
char cdata[1];
//data[0] = data_in;
defADC1263_CSPin_Clr;
Delay_ms(2);
defADC1263_CSPin_Set;
Delay_ms(2);
defADC1263_CSPin_Clr;
Delay_ms(2);
SPI3_Write (data_in);
Delay_ms(2);
defADC1263_CSPin_Set;
}
//Sends a write command to SCP1000
void ads1262_Reg_Write (unsigned char READ_WRITE_ADDRESS, unsigned char DATA){
char dataToSend;
// now combine the register address and the command into one byte:
dataToSend = READ_WRITE_ADDRESS | WREG;
defADC1263_CSPin_Clr;
Delay_ms(2);
defADC1263_CSPin_Set;
Delay_ms(2);
// take the chip select low to select the device:
defADC1263_CSPin_Clr;
Delay_ms(2);
SPI3_Write (dataToSend); //Send register location
SPI3_Write (0x00); //number of register to wr
SPI3_Write (DATA); //Send value to record into register
Delay_ms(2);
// take the chip select high to de-select:
defADC1263_CSPin_Set;
}
char ADCS_DRDY_Status(){
char ucStatus;
if(defADC1263_GetPinStatusDRDY == 0) // monitor Data ready(DRDY pin)
{
ucStatus = 1;
}
else {
ucStatus = 0;
}
return ucStatus;
}
There is some ADS1263 example code that was released along with the TIPD188 reference design. Please, refer to the "TIPD188 Firmware" download, under the "Software" section. I hope that helps you out! Best regards, Chris