Part Number: AFE4400
Other Parts Discussed in Thread: MSP430F5529,
We have interfaced AFE4400 to MSP430F5529 as per AFE4400SPO2EVM. As we are program it by using the code of AFE4400SPO2EVM , The LED'S of SPO2 probe are blinking as on the Test point (Pins of DB9 connector voltage is fluctuating from 1.2v to 4V ) I this there is a only program issue because as in same if we program it by other sample code then on DB9 pin voltage is constant ie. 1.2v arround but LEDs are off. So what are the changes in the program please suggest.
/* * AFE44x0.c * * Provides AFE44x0 API * * Copyright (C) 2016 Texas Instruments Incorporated - http://www.ti.com/ * ALL RIGHTS RESERVED * */ #include "device.h" #include "types.h" //Basic Type declarations #include "AFE44x0.h" /************************************************************************************************************************************************** * Prototypes * **************************************************************************************************************************************************/ /************************************************************************************************************************************************** * Global Variables * **************************************************************************************************************************************************/ #define DELAY_COUNT 2 unsigned long AFE44xx_Current_Register_Settings[36] = { CONTROL0_VAL, //Reg0:CONTROL0: CONTROL REGISTER 0 LED2STC_VAL, //Reg1:REDSTARTCOUNT: SAMPLE RED START COUNT LED2ENDC_VAL, //Reg2:REDENDCOUNT: SAMPLE RED END COUNT LED2LEDSTC_VAL, //Reg3:REDLEDSTARTCOUNT: RED LED START COUNT LED2LEDENDC_VAL, //Reg4:REDLEDENDCOUNT: RED LED END COUNT ALED2STC_VAL, //Reg5:AMBREDSTARTCOUNT: SAMPLE AMBIENT RED START COUNT ALED2ENDC_VAL, //Reg6:AMBREDENDCOUNT: SAMPLE AMBIENT RED END COUNT LED1STC_VAL, //Reg7:IRSTARTCOUNT: SAMPLE IR START COUNT LED1ENDC_VAL, //Reg8:IRENDCOUNT: SAMPLE IR END COUNT LED1LEDSTC_VAL, //Reg9:IRLEDSTARTCOUNT: IR LED START COUNT LED1LEDENDC_VAL, //Reg10:IRLEDENDCOUNT: IR LED END COUNT ALED1STC_VAL, //Reg11:AMBIRSTARTCOUNT: SAMPLE AMBIENT IR START COUNT ALED1ENDC_VAL, //Reg12:AMBIRENDCOUNT: SAMPLE AMBIENT IR END COUNT LED2CONVST_VAL, //Reg13:REDCONVSTART: REDCONVST LED2CONVEND_VAL, //Reg14:REDCONVEND: RED CONVERT END COUNT ALED2CONVST_VAL, //Reg15:AMBREDCONVSTART: RED AMBIENT CONVERT START COUNT ALED2CONVEND_VAL, //Reg16:AMBREDCONVEND: RED AMBIENT CONVERT END COUNT LED1CONVST_VAL, //Reg17:IRCONVSTART: IR CONVERT START COUNT LED1CONVEND_VAL, //Reg18:IRCONVEND: IR CONVERT END COUNT ALED1CONVST_VAL, //Reg19:AMBIRCONVSTART: IR AMBIENT CONVERT START COUNT ALED1CONVEND_VAL, //Reg20:AMBIRCONVEND: IR AMBIENT CONVERT END COUNT ADCRSTSTCT0_VAL, //Reg21:ADCRESETSTCOUNT0: ADC RESET 0 START COUNT ADCRSTENDCT0_VAL, //Reg22:ADCRESETENDCOUNT0: ADC RESET 0 END COUNT ADCRSTSTCT1_VAL, //Reg23:ADCRESETSTCOUNT1: ADC RESET 1 START COUNT ADCRSTENDCT1_VAL, //Reg24:ADCRESETENDCOUNT1: ADC RESET 1 END COUNT ADCRSTSTCT2_VAL, //Reg25:ADCRESETENDCOUNT2: ADC RESET 2 START COUNT ADCRSTENDCT2_VAL, //Reg26:ADCRESETENDCOUNT2: ADC RESET 2 END COUNT ADCRSTSTCT3_VAL, //Reg27:ADCRESETENDCOUNT3: ADC RESET 3 START COUNT ADCRSTENDCT3_VAL, //Reg28:ADCRESETENDCOUNT3: ADC RESET 3 END COUNT PRP, //Reg29:PRPCOUNT: PULSE REPETITION PERIOD COUNT CONTROL1_VAL, //Reg30:CONTROL1: CONTROL REGISTER 1 //timer enabled, averages=3, RED and IR LED pulse ON PD_ALM AND LED_ALM pins 0x00000, //Reg31:?: ?? (ENSEPGAIN + STAGE2EN_LED1 + STG2GAIN_LED1_0DB + CF_LED1_5P + RF_LED1_1M), //Reg32:TIAGAIN: TRANS IMPEDANCE AMPLIFIER GAIN SETTING REGISTER (AMBDAC_0uA + FLTRCNRSEL_500HZ + STAGE2EN_LED2 + STG2GAIN_LED2_0DB + CF_LED2_5P + RF_LED2_1M), //Reg33:TIA_AMB_GAIN: TRANS IMPEDANCE AAMPLIFIER AND AMBIENT CANELLATION STAGE GAIN (LEDCNTRL_VAL), //Reg34:LEDCNTRL: LED CONTROL REGISTER (TX_REF_1 + RST_CLK_ON_PD_ALM_PIN_DISABLE + ADC_BYP_DISABLE + TXBRGMOD_H_BRIDGE + DIGOUT_TRISTATE_DISABLE + XTAL_ENABLE + EN_FAST_DIAG + PDN_TX_OFF + PDN_RX_OFF + PDN_AFE_OFF) //Reg35:CONTROL2: CONTROL REGISTER 2 //bit 9 }; /*********************************************************************************************************** * Variables for the SPI Interaction * ***********************************************************************************************************/ /********************************************************************************************************** * External Variables * **********************************************************************************************************/ /********************************************************************************************************** * Init_AFE44xx_DRDY_Interrupt * **********************************************************************************************************/ void Init_AFE44xx_DRDY_Interrupt (void) { P2DIR &= ~AFE_ADC_DRDY; P2REN |= AFE_ADC_DRDY; // Enable P2.3 internal resistance P2OUT |= AFE_ADC_DRDY; // Set P2.3 as pull-Up resistance P2IES |= AFE_ADC_DRDY; // P2.3 Hi/Lo edge P2IFG &= ~AFE_ADC_DRDY; // P2.3 IFG cleared P2IE &= ~AFE_ADC_DRDY; // P2.3 interrupt disabled } /********************************************************************************************************** * Enable_AFE44xx_DRDY_Interrupt * **********************************************************************************************************/ void Enable_AFE44xx_DRDY_Interrupt (void) { P2IFG &= ~AFE_ADC_DRDY; // P2.3 IFG cleared P2IE |= AFE_ADC_DRDY; // P2.3 interrupt enabled } /********************************************************************************************************** * Disable_AFE44xx_DRDY_Interrupt * **********************************************************************************************************/ void Disable_AFE44xx_DRDY_Interrupt (void) { P2IFG &= ~AFE_ADC_DRDY; // P2.3 IFG cleared P2IE &= ~AFE_ADC_DRDY; // P2.3 interrupt disabled } /********************************************************************************************************** * Set_GPIO * **********************************************************************************************************/ void Set_GPIO(void) { //port set.. //Port 1.1 - AFE_RESETZ, P1.2 - AFE_PDNZ, P2.3 - ADC_RDY, P2.4- PD_ALM, P2.5 - LED_ALM, //P5.7 - DIAG_END P1SEL |= BIT0; P1DIR |= BIT0; P1OUT |= BIT0; P1DIR |= (AFE_RESETZ + AFE_PDNZ); P1OUT |= (AFE_RESETZ + AFE_PDNZ); P2DIR &= ~(AFE_ADC_DRDY + AFE_PD_ALM + AFE_LED_ALM); P5DIR &= ~AFE_DIAG_END; P2SEL = 0x00; P2DIR &= BIT0; P2OUT |= (BIT1 + BIT2 + BIT7); P2DIR |= (BIT1 | BIT2 | BIT7); } /********************************************************************************************************** * Set_UCB1_SPI * **********************************************************************************************************/ void Set_UCB1_SPI(void) { P4SEL |= BIT1+BIT2+BIT3; // Set SPI peripheral bits P4DIR |= BIT0+BIT1+BIT3; // STE, SCLK, and DOUT as output P4DIR &= ~BIT2; // Din as input P4OUT |=BIT0; // Set STE high UCB1CTL1 |= UCSWRST; // Enable SW reset UCB1CTL0 |= UCMSB+UCCKPH+UCMST+UCSYNC; // [b0] 1 - Synchronous mode // [b2-1] 00- 3-pin SPI // [b3] 1 - Master mode // [b4] 0 - 8-bit data // [b5] 1 - MSB first // [b6] 0 - Clock polarity high. // [b7] 1 - Clock phase - Data is captured on the first UCLK edge and changed on the following edge. UCB1CTL1 |= UCSSEL_2; // SMCLK UCB1BR0 = 0x01; // 16 MHz UCB1BR1 = 0; // UCB1CTL1 &= ~UCSWRST; // Clear SW reset, resume operation UCB1IE =0x0; //P4OUT &= ~BIT0; // Set STE low } /********************************************************************************************************** * Init_AFE44xx_Resource * **********************************************************************************************************/ void Init_AFE44xx_Resource(void) { Set_GPIO(); // Initializes AFE44xx's input control lines Set_UCB1_SPI(); // Initialize SPI regs. } /********************************************************************************************************** * AFE44xx default Initialization * **********************************************************************************************************/ void AFE44xx_Default_Reg_Init(void) { Disable_AFE44x0_SPI_Read(); AFE44x0_Reg_Write((unsigned char)PRPCOUNT, (unsigned long)PRP); AFE44x0_Reg_Write((unsigned char)LED2STC, (unsigned long)LED2STC_VAL); AFE44x0_Reg_Write((unsigned char)LED2ENDC, (unsigned long)LED2ENDC_VAL); AFE44x0_Reg_Write((unsigned char)LED2LEDSTC, (unsigned long)LED2LEDSTC_VAL); AFE44x0_Reg_Write((unsigned char)LED2LEDENDC, (unsigned long)LED2LEDENDC_VAL); AFE44x0_Reg_Write((unsigned char)ALED2STC, (unsigned long)ALED2STC_VAL); AFE44x0_Reg_Write((unsigned char)ALED2ENDC, (unsigned long)ALED2ENDC_VAL); AFE44x0_Reg_Write((unsigned char)LED1STC, (unsigned long)LED1STC_VAL); AFE44x0_Reg_Write((unsigned char)LED1ENDC, (unsigned long)LED1ENDC_VAL); AFE44x0_Reg_Write((unsigned char)LED1LEDSTC, (unsigned long)LED1LEDSTC_VAL); AFE44x0_Reg_Write((unsigned char)LED1LEDENDC, (unsigned long)LED1LEDENDC_VAL); AFE44x0_Reg_Write((unsigned char)ALED1STC, (unsigned long)ALED1STC_VAL); AFE44x0_Reg_Write((unsigned char)ALED1ENDC, (unsigned long)ALED1ENDC_VAL); AFE44x0_Reg_Write((unsigned char)LED2CONVST, (unsigned long)LED2CONVST_VAL); AFE44x0_Reg_Write((unsigned char)LED2CONVEND, (unsigned long)LED2CONVEND_VAL); AFE44x0_Reg_Write((unsigned char)ALED2CONVST, (unsigned long)ALED2CONVST_VAL); AFE44x0_Reg_Write((unsigned char)ALED2CONVEND, (unsigned long)ALED2CONVEND_VAL); AFE44x0_Reg_Write((unsigned char)LED1CONVST, (unsigned long)LED1CONVST_VAL); AFE44x0_Reg_Write((unsigned char)LED1CONVEND, (unsigned long)LED1CONVEND_VAL); AFE44x0_Reg_Write((unsigned char)ALED1CONVST, (unsigned long)ALED1CONVST_VAL); AFE44x0_Reg_Write((unsigned char)ALED1CONVEND, (unsigned long)ALED1CONVEND_VAL); AFE44x0_Reg_Write((unsigned char)ADCRSTSTCT0, (unsigned long)ADCRSTSTCT0_VAL); AFE44x0_Reg_Write((unsigned char)ADCRSTENDCT0, (unsigned long)ADCRSTENDCT0_VAL); AFE44x0_Reg_Write((unsigned char)ADCRSTSTCT1, (unsigned long)ADCRSTSTCT1_VAL); AFE44x0_Reg_Write((unsigned char)ADCRSTENDCT1, (unsigned long)ADCRSTENDCT1_VAL); AFE44x0_Reg_Write((unsigned char)ADCRSTSTCT2, (unsigned long)ADCRSTSTCT2_VAL); AFE44x0_Reg_Write((unsigned char)ADCRSTENDCT2, (unsigned long)ADCRSTENDCT2_VAL); AFE44x0_Reg_Write((unsigned char)ADCRSTSTCT3, (unsigned long)ADCRSTSTCT3_VAL); AFE44x0_Reg_Write((unsigned char)ADCRSTENDCT3, (unsigned long)ADCRSTENDCT3_VAL); AFE44x0_Reg_Write((unsigned char)CONTROL0, AFE44xx_Current_Register_Settings[0]); //0x00 AFE44x0_Reg_Write((unsigned char)CONTROL2, AFE44xx_Current_Register_Settings[35]); //0x23 AFE44x0_Reg_Write((unsigned char)TIAGAIN, AFE44xx_Current_Register_Settings[32]); //0x20 AFE44x0_Reg_Write((unsigned char)TIA_AMB_GAIN, AFE44xx_Current_Register_Settings[33]); //0x21 AFE44x0_Reg_Write((unsigned char)LEDCNTRL, AFE44xx_Current_Register_Settings[34]); //0x22 AFE44x0_Reg_Write((unsigned char)CONTROL1, AFE44xx_Current_Register_Settings[30]); //0x1E Enable_AFE44x0_SPI_Read(); } /********************************************************************************************************** * AFE44xx_Read_All_Regs * **********************************************************************************************************/ void AFE44xx_Read_All_Regs(unsigned long AFE44xxeg_buf[]) { unsigned char Regs_i; for ( Regs_i = 0; Regs_i < 50; Regs_i++) { AFE44xxeg_buf[Regs_i] = AFE44xx_Reg_Read(Regs_i); } } /*********************************************************************************************************/ /********************************************************************************************************** * AFE44xx_PowerOn_Init * ***********************************************************************************************************/ void AFE44xx_PowerOn_Init(void) { volatile unsigned short Init_i, j; Init_AFE44xx_Resource(); for (j = 0; j < DELAY_COUNT; j++) { for ( Init_i =0; Init_i < 20000; Init_i++); for ( Init_i =0; Init_i < 20000; Init_i++); for ( Init_i =0; Init_i < 20000; Init_i++); } Init_AFE44xx_DRDY_Interrupt(); AFE44xx_Default_Reg_Init(); } /********************************************************************************************************** * AFE44x0_Reg_Write * ***********************************************************************************************************/ void AFE44x0_Reg_Write (unsigned char reg_address, unsigned long data) { unsigned char dummy_rx; P4OUT&= ~0x01; // SEN LOW FOR TRANSMISSION. // Loop unrolling for machine cycle optimization UCB1TXBUF = reg_address; // Send the first byte to the TX Buffer: Address of register while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = (unsigned char)(data >>16); // Send the second byte to the TX Buffer: Data[23:16] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = (unsigned char)(((data & 0x00FFFF) >>8)); // Send the third byte to the TX Buffer: Data[15:8] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = (unsigned char)(((data & 0x0000FF))); // Send the first byte to the TX Buffer: Data[7:0] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf P4OUT|=0x01; // SEN HIGH } /********************************************************************************************************** * AFE44x0_Reg_Read * ***********************************************************************************************************/ unsigned long AFE44x0_Reg_Read(unsigned char Reg_address) { unsigned char SPI_Rx_buf[4]; unsigned long retVal; retVal = 0; P4OUT&= ~0x01; // SEN LOW FOR TRANSMISSION. // Loop unrolling for machine cycle optimization UCB1TXBUF = Reg_address; // Send the first byte to the TX Buffer: Address of register while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? SPI_Rx_buf[0] = UCB1RXBUF; // Read Rx buf UCB1TXBUF = 0; // Send the second byte to the TX Buffer: dummy data while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? SPI_Rx_buf[1] = UCB1RXBUF; // Read Rx buf: Data[23:16] UCB1TXBUF = 0; // Send the third byte to the TX Buffer: dummy data while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? SPI_Rx_buf[2] = UCB1RXBUF; // Read Rx buf: Data[15:8] UCB1TXBUF = 0; // Send the first byte to the TX Buffer: dummy data while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? SPI_Rx_buf[3] = UCB1RXBUF; // Read Rx buf: Data[7:0] P4OUT|=0x01; // set HIGH at end of transmission retVal = SPI_Rx_buf[1]; retVal = (retVal << 8) | SPI_Rx_buf[2]; retVal = (retVal << 8) | SPI_Rx_buf[3]; //retVal = (SPI_Rx_buf[1]<<16)|(SPI_Rx_buf[2]<<8)|(SPI_Rx_buf[3]); return retVal; } /********************************************************************************************************** * Enable_AFE44x0_SPI_Read * **********************************************************************************************************/ void Enable_AFE44x0_SPI_Read (void) { unsigned char dummy_rx; //Set Control0 - Enable SPI Read bit P4OUT&= ~0x01; // CS LOW for start of transmission. // Loop unrolling for machine cycle optimization UCB1TXBUF = 0; // Send the first byte to the TX Buffer: Address of register while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = 0; // Send the second byte to the TX Buffer: Data[23:16] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = 0; // Send the third byte to the TX Buffer: Data[15:8] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = 1; // Send the first byte to the TX Buffer: Data[7:0] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf P4OUT|=0x01; // CS High for end of transmission } /********************************************************************************************************** * Disable_AFE44x0_SPI_Read * **********************************************************************************************************/ void Disable_AFE44x0_SPI_Read (void) { unsigned char dummy_rx; //Set Control0 - Disable SPI Read bit P4OUT&= ~0x01; // CS LOW for start of transmission. // Loop unrolling for machine cycle optimization UCB1TXBUF = 0; // Send the first byte to the TX Buffer: Address of register while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = 0; // Send the second byte to the TX Buffer: Data[23:16] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = 0; // Send the third byte to the TX Buffer: Data[15:8] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf UCB1TXBUF = 0; // Send the first byte to the TX Buffer: Data[7:0] while ( (UCB1STAT & UCBUSY) ); // USCI_B1 TX buffer ready? dummy_rx = UCB1RXBUF; // Dummy Read Rx buf P4OUT|=0x01; // CS High for end of transmission } /*********************************************************************************************************/ /**********************************************************************************************************/ // Echo character #pragma vector=USCI_B1_VECTOR __interrupt void USCI_B1_ISR(void) { switch(UCB1IV) { case 0:break; // Vector 0 - no interrupt case 2:break; // Vector 2 - RXIFG case 4:break; // Vector 4 - TXIFG default: break; } } // End of file