Hi team,
We would like to understand the definition of TUE in DAC8750 datasheet.
1. Does TUE specification include INL, Offset Error and Gain Error?
We are confused this because the datasheet has TUE and also INL, Offset Error and Gain Error.
2. There are two case of TUE in DAC8750 datasheet, (0 mA TO 20 mA AND 0 mA TO 24 mA) and (4 mA TO 20 mA).
In case of (0 mA TO 20 mA AND 0 mA TO 24 mA), does this include internal Rset error?
In case of (4 mA TO 20 mA), there are two case specification, Internal Rset or External Rset in the datasheet. What is test condition of these resisters?
I understand these errors would affect TUE.
Regards,
Noriyuki Takahashi