Part Number: ADS8638
Hi,
My customer design ADS8638 as below cirucuit, and the power source is described in below figure.
Their application is vibration.
The input signal is 3.3V from power supply.
Sampling Frequency is 25KHz.
And they found that there is a spurious appear at 91Hz if they use ADS8638.
At the same conditions, there is no spurious if they use ADI AD4000
Test results are shown as below.
Could you give us some advice to avoid the 91Hz spurious ?
TI ADS8638
ADI AD4000