Tool/software: Code Composer Studio
Hi, I am working on the SPI code to transfer data from the PGA970EVM board to my Digital Interface. I already created the code to synch both devices, and move the data to the COMBUF registers. I can see the DIF writing to the register COM_DIF_TO_MCU. However, when I check the transmission using the Logic Analyzer I don't see the 0x05 at the beginning of the communication. I tried to enable the SPI communication using the following commands
DIG_IF_CTRL = 0x00;
MICRO_INTERFACE_CONTROL = 0x00;
But the only thing that it happened is that the board got locked in reset mode. The Logic Analyzer and the MCU are configured in SPI MODE 1. Could someone help us figure out what is going on? It feels that something is missing or a configuration is missing, but we are not able to find it.
Thanks,
Hector