This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45: ADC32RF45EVM Xilinx Vivado project

Part Number: ADC32RF45
Other Parts Discussed in Thread: LMK04828, LMX2582,

Hello,

I have the ADC32RF45EVM and a selection of Xilinx Ultrascale and 7-series boards. I have successfully used the eval software and the Xilinx ZC706 to prove that the ADC is working properly.

The next step is to build a Vivado project that targets the EVM, and write a basic driver that configures the ADC32RF45 itself, the LMK04828, and the LMX2582 synthesizer.

The software driver settings I can get via register dumps from the TI GUIs. However, is there a Vivado project that can be used for reference? How would one get it, or get the source of the eval design that TI provides in a bitfile?

Thanks!