Part Number: LMP90100
My question pertains to the LMP90100MH/NOPB 24-bit ADC.
For our application, we’re using the ADC’s internal 893kHZ clock for sampling. What is the frequency stability of this clock?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMP90100
My question pertains to the LMP90100MH/NOPB 24-bit ADC.
For our application, we’re using the ADC’s internal 893kHZ clock for sampling. What is the frequency stability of this clock?
Mark,
It looks like there was some characterization done on the internal oscillator frequency. Looking at final test data on just under 300000 units, the average frequency was 893kHz, with the great majority between 891 and 896, there are some flyers that push this out to 880 and 909, but those are removed by final test:
Measuring units over temperature, there is also some variation as the temperature rises.
Joseph Wu