I am fairly new to this concept so bear with me if I made a mistake or am unclear about something.
I am designing a DC kWh meter for my internship. The voltage which has to be measured is going to be 5VDC after a voltage divider and the current that is going to be measured is 20A using a LPSR 15-NP Hall effect sensor.
I was wondering if the ADS1115 is a good choice for my application or if I should use another ADC. I have studied the datasheet but it is unclear to me what the FSR is. How do I determine what my FSR is. My VDD is 5V so do I use the 6.144V or the 4.096V. I need to know this because I want to know what the effect of the Zcm is on the voltage divider. That way I can calculate the voltage that the ADC sees.
I thank you in advance and hope I have informed well.