Our system consists of ADS5294s across 4 different modules that can be powered up and programmed separately as the system is brought up.
However, once the sampling process starts, we are under the impression that as long as there is no decimation, and assuming that the sample clocks and input signals applied to each ADC are coherent, we should NOT require the use of the SYNC input to synchronize the 4 ADCs.
What we see is that the outputs (looking across all the ADCs) can be off by a sample (sampling at 20MHz or 40MHz).
We then modified our system to allow for a SYNC to be applied to all ADCs simultaneously and when we encountered this one sample skew, applied the SYNC and found the resulting data to now become aligned.
We were surprised by this as the SYNC descriptions in the data sheet and any forums I've read only apply to requiring SYNC for decimation. So my question is: are there any other situations where SYNC should be used and does the scenario we encountered above make sense?
Thanks,
Bob