Other Parts Discussed in Thread: AFE5801, CDCE62002, AFE5808A
Hello TI Team,
I am using AFE5801 for one of my project and I have following questions :
(1) I would like to know the differential impedance with which the input Analog signals (differential) be routed. Any recommendation on trace width and spacing that you advise?
(2) I am only using 6 channels at the moment. What do you recommend to do with the unused Analog inputs ? Similarly, what would you recommend to do with the unused LVDS outputs of corresponding unused analog channels
(3) To what supply are the signals PDN, RESET, SCLK, SDATA, SEN# referenced to ? In data sheet the maximum Input voltage on these pins is written as 3.6V and similarly for SDOUT it is mentioned as 1.8V? Can you please clarify this since I am driving these signals from an FPGA bank with 3.3V supply.
(4) The signals PDN, RESET, SCLK, SDATA, SEN# need any external pull up/down resistors ? If so, to what supply should the pull up be referenced ?
Looking forward to your reply.
Thanks
Nikhil