This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3482: No Output

Part Number: DAC3482

I have been unsuccessful in configuring the DAC3482 EVM to produce an analog output signal.  I just need a minimalist configuration to produce an analog output from 8-bit digital input with the following parameters:

DACCLK: 1GHz

DATACLK: 125MHz

Data Interface: Byte-Wide, D[7:0] (D[15:8] are tied off)

FIFO In Sync:  FRAME (No parity, pulse every 8 samples)
FIFO Out Sync: FRAME
Data Format:   FRAME

Input Format: 8-bit Dual mode, 2's Compliment
Data Delay: 200ps
Clock Delay: 0ps

PLL: Disabled

Interpolation: 1x
Digital Mixer: Bypass

  • Hi Michael,

    Unfortunately, the DAC3482 in 8-bit LVDS bus mode only support up to 312.5MSPS of baseband input rate. This is limited by the LVDS bus rate of 1250Mbps.

    This means that with 1GSPS of DACCLK, you will need to enable the 4x interpolation mode with 250MSPS of input rate at the 8-bit LVDS bus. You cannot use 1x interpolation in this case.

    We also recommend using the dataclk delay instead of the data delay. The use of data delay will also shift the delay of the FRAME signal with respect to the DATACLK, and hence this may not be able to create the setup/hold time delay with respect to the DATA + FRAME to the DATACLK depending on your logic implementation.

    Let me know if the 4x interpolation would work for you.

    -Kang
  • Waiting for user feedback....
  • I am supplying a 1GHz clock to EVM CLKIN (J9) have an input data rate of 62.5Msps so am setting interpolation to 16x, but still no output.  See attached DAC3482 EVM register configuration file.

       x00	   xF88C
       x01	   x0000
       x02	   x0042
       x03	   xF001
       x04	   x5DFD
       x05	   x0260
       x06	   x2500
       x07	   xFFFF
       x08	   x0000
       x09	   x8000
       x0A	   x0000
       x0B	   x0000
       x0C	   x07FF
       x0D	   x07FF
       x0E	   x05A6
       x0F	   x05A6
       x10	   x3000
       x11	   x0000
       x12	   x0000
       x13	   x0000
       x14	   x0000
       x15	   x0640
       x16	   x0000
       x17	   x0640
       x18	   x205F
       x19	   x10F4
       x1A	   x4820
       x1B	   x0800
       x1C	   x0000
       x1D	   x0000
       x1E	   x1111
       x1F	   x8882
       x20	   x2400
       x22	   x1B1B
       x23	   x001F
       x24	   x1000
       x25	   x7A7A
       x26	   xB6B6
       x27	   xEAEA
       x28	   x4545
       x29	   x1A1A
       x2A	   x1616
       x2B	   xAAAA
       x2C	   xC6C6
       x2D	   x0004
       x2E	   x0000
       x2F	   x0000
       x30	   x61A8
       x7F	   x0004
    CDCE62005 Registers
    Freq:19.200000MHz
    Address	Data
    00		80400000
    01		813C0001
    02		81400002
    03		C10C0003
    04		81400004
    05		29F01A55
    06		44AF0006
    07		165294A7
    08		20001808

  • Hi Michael,

    I will take a look in the next few days.

    Could you confirm how you are interfacing with the DAC3482 EVM? Through the TSW1400 Pattern Generator and HSDC PRO?

    -Kang

  • Yes, I'm using the TSW1400 and HSDC Pro on the evaluation platform.  But I've received this hardware second-hand and am beginning to suspect there might be an issue with it.  However, I did make a little progress on my real hardware yesterday.  Once I set the interpolation rate correctly (16x), I began seeing something coming out of the DAC.  The analog signal doesn't look correct, but at least I'm getting a signal.  I have an FPGA that is driving the SPI interface and generating the DDR data into the DAC.  I'm going to set the EVM aside today and focus on making addition progress on my hardware.

    My original goal with the EVM hardware was to quickly find a simple configuration of the DAC that would allow me to route data through the part without the NCO.  I planned to code up those register settings and write them out to the DAC SPI on my hardware.  This would put my DAC in a verified functional configuration so I could focus on debugging the FPGA data interface.  If you could take the DAC configuration file that I uploaded and look at it in the DAC3482 EVM software and verify that I don't have something configured incorrectly, that would be very helpful.  Thanks.

  • Hi Kang,

    Any concerns about the DAC3482 configuration file I uploaded?

    --Michael

  • Hi Michael,

    I have not yet gotten the 8bit bus mode to work. I hope the TSW1400 FPGA firmware update didn't break the 8bit bus mode configuration from the FPGA side.

    I have made the 16-bit bus mode at 16x interpolation to work. You can see the ppt file for my setup and also the configuration file attached. I will try again on the 8bit mode.DAC3482 Setup.pptxhttps://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/73/DAC3482_5F00_16bitbus_5F00_16x_5F00_NCO30MHz_5F00_1000MSPS

  • Hi Michael,

    Please see below for verified script and HSDC PRO setup. I will close this post for now and you can always reply if you have additional questions

    -Kang

    DAC3482 Byte Wise Operation.pptx

       x00	   xF888
       x01	   x0800
       x02	   x0052
       x03	   xA001
       x04	   xFFFF
       x05	   x0060
       x06	   x2D00
       x07	   xFFFF
       x08	   x0000
       x09	   x8000
       x0A	   x0000
       x0B	   x0000
       x0C	   x05A6
       x0D	   x05A6
       x0E	   x05A6
       x0F	   x05A6
       x10	   x3000
       x11	   x0000
       x12	   x0000
       x13	   x0000
       x14	   x28F6
       x15	   x0F5C
       x16	   x28F6
       x17	   x0F5C
       x18	   x205F
       x19	   x10F4
       x1A	   x4820
       x1B	   x0800
       x1C	   x0000
       x1D	   x0000
       x1E	   x1111
       x1F	   x8880
       x20	   x2201
       x22	   x1B1B
       x23	   x001F
       x24	   x1000
       x25	   x7A7A
       x26	   xB6B6
       x27	   xEAEA
       x28	   x4545
       x29	   x1A1A
       x2A	   x1616
       x2B	   xAAAA
       x2C	   xC6C6
       x2D	   x0004
       x2E	   x0000
       x2F	   x0000
       x30	   x61A8
       x7F	   x0004
    CDCE62005 Registers
    Freq:19.200000MHz
    Address	Data
    00		80400000
    01		813C0001
    02		81400002
    03		C11C0003
    04		C11C0004
    05		29F01A55
    06		44AF0006
    07		165294A7
    08		20001808

  • Thanks, Kang.  I have downloaded and tested both your 16-bit and 8-bit (byte-wise) configuration files and still do not see any output from the DAC.  This further confirms that I am having some issues with the EVM hardware that I am working with.  I will see to obtaining a new EVM system before proceeding further.  Thanks again for you help with this.

  • Hi Michael,

    Could you please check the EVM Jumper to see if it matches with the user's guide recommendation? If some of the jumpers are inconsistent, you may not be able to get an output too. Perhaps it is a last resort before you order another EVM.

  • Hi Kang,

    I have verified the jumper setting on the EVM, and they match the default settings shown in the table that you provided.

    Thanks,

    Michael