This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3283EVM: DAC EVM with DC coupling to work together with VC707

Part Number: DAC3283EVM
Other Parts Discussed in Thread: ADS5400EVM, ADS5400, ADS54J40, ADC12J4000

Good day.

My current setup is DAC3283EVM + ADS54EVM (TSW4200) + Xilinx VC707

Can you recommend a suitable ADC/DAC with DC coupling as replacement? (TSW4200 is obselete).

Thanks & regards.

  • Doreen:

    There may be a few options. First off, you can still acquire the DAC3283EVM and the ADS5400EVM. The individual EVMs are not obsolete. If additional adapter cards are needed then your local sales support team will be able to help acquire an additional board from factory/lab stock.

    You can consider switching to the DAC348xEVM. This is a higher sampling rate dual or quad with LVDS interface. You can consider ADS42xx ADCs if 250 MSPS or less is needed. If 1 GHz sampling rate with LVDS interface is needed the ADS5400 is still a good choice.

    If you can switch to a JESD204B interface there are some additional options. You can check out the TSW40RF80 which is an RF sampling transceiver. The ADC however does not support DC interface. You can check out other options like ADC12J4000 that do support or ADS54J40.

    I encourage you to contact your local sales support team and they can give a more comprehensive look at your options once they know the requirements for your case.

    --RJH
  • RJH, thanks for your prompt reply. We have contacted our sales support.