Part Number: DAC37J84EVM
Hi,
I would like to test DAC37J84EVM with Xilinx FPGA part no: ZCU102.
Is it possible to connect both cards without Interposer card? If yes, then please check & confirm the below configuration.
1) Connected DAC37J84EVM & FPGA card directly through FMC connectors.
2) Connected external SYNC (single ended) from DAC i.e., J21 - 1 & 3 pins to FPGA J55 - 1& 3 pins. For our end project purpose we need SYNC as Single Ended only.
Best Regards,
Swarup.