Part Number: DAC8718
HI, I'm testing DAC8718.
I got a problem that DAC8718 outputs error after power-on, the error output is zero and the right ourput is -15V. then It always outputs +15V when I try to control it.
Before, due to the unusual sag in the 15V and 5V power up process,the anomaly occurred. So I adjust power-on sequencing.
CH1 is 3.3V for IOVDD,CH2 is 5V for DVDD, , CH3 is +15V for AVDD, CH4 is -15V for AVSS
It is meeting the manual sequencing requirements.
At the same time, I tested the voltage of OFFSET.
OFFSET-A is 0V
OFFSET-B is 2.983V.
Thanks for reading.