This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1306M05: Is there a const-sensitive,non-isolated version available?

Part Number: AMC1306M05
Other Parts Discussed in Thread: AMC1035, ADS1203, ADS1202

Is there a const-sensitive,non-isolated version available?

Just w/o the isolator integrated?

  • Hi Urs,

    Welcome to our e2e Forum! There are devices like the ADS1202 and ADS1203 which both feature +/-250mV input ranges and are non-isolated, but they come in a slightly larger package. The is also the AMC1035, but that has a significantly higher input voltage range. What sort of application are you needing the 50mV non-isolated modulator for.