Part Number: ADS54J20EVM
Other Parts Discussed in Thread: ADS54J20
In the reference schematics, we are seeing some intermediate voltage transitions to generate the needed voltage for the DAC. Any specific reason for this? Is it mandate to follow in our application circuitry? Please share your feedback. Your timely response is highly appreciable.
Following are the power tree:
5V---> 3.7V-->3.3V--->DAC
5V---> 3.7V---> 3.0V--->DAC
5V--> 2.3V-->1.9---> DAC
2.3V--->1.9V--> DAC
2.3V--->1.15V---> DAC
Thank you,
K.Harsha