Other Parts Discussed in Thread: ADS1120, PGA300, ADS112C04, ADS122C04, ADS1234
Hi Team,
I am looking for strain-gauge Load cell Analog to Digital Converter which will be used with below specified Load cell module.
Specs:
1) Excitation Voltage-- > 3~10V
2) Rated Output------- > 2.0 ± 0.15 mV/V
3) Input resistance---- > 385 ± 10 Ohm
4) Output Resistance--- > 385 ± 10 Ohm
5) Capacity--------------- > 150 Kg
Please let me know any cheaper and best suitable Ic which can work on I2C interface with Host.
I have seen some Ic which are PGA300 and ADS1120 . ADS1120 is based on SPI interface which is not suitable for me and on other hand PGA300 is with inbuilt SOC but this is expensive.
So, let me know any best suitable part.