Part Number: DAC8734EVM
I have set up an SPI bus interface between a PSoC 5lp processor and a TI8734EVM board. I can write perfectly to all four of the 8734 DAC channels. However, when I send a read command querying the DAC input registers (or latch registers), followed by a NOP command to push bits out of the SPI shift register, the SDO returns an immediate echo of the bits that I am sending to the SDI. This is exactly the behavior that Yelsing Torres reports in his thread. Unfortunately, that thread stops without arriving at any conclusion. Can you help? Thanks so much.