Hi Team,
My customer considers to use DAC80508 DSBGA package(2.4mm x 2.4mm).
He concerns if the device is usable without damaging under following conditions.
-------------------------------------
Ta: 95°C
output current: 20mA(DC) x 8ch
output voltage: 2.5V x 8ch
VDD: 5.5V
-------------------------------------
May I have your advice?
Best Regards,
Yaita