Part Number: ADS1257
Hi,
Let me ask you some basic questions about ADS1257 as below.
Q1) INL specifications
Following is a part of System performace table (data sheet page 7)
Q1-1) About INL, the value is only "+", there is no "-" value, +3ppm(typ)/+10ppm(max).
I suppose that it should be described as "+/-" value, that is to say, +/-3ppm(typ), +/-10ppm(max).
What do you think of my idea?
If INL has only "+" value, it seems to be strange that "Gain error" has "+/-" value, +/-0.005%.
Q1-2) About INL value, the specification is defined "after calibration(Gain/offset, self)", correct?
And is this value from "END-Point" method, right?
Q1-3) INL curve
Following is the INL data, Fig19/page 12.
I have a question about the "shape" of INL curve.
The Shape seems to show around "inverse S" curve, not random.
Will you tell me the reason why INL shows such kind of shape like "S"?
I suppose that not only ADS1257 but also other delta-sigma A/D has similat curve...it's my feeling, sorry.
Q2) ENOB, NFB
You use "RMS" noise and "peak to peak" noise to calculate ENOB and NFB.
About the noise, how did you get them?
Did you measure them by like "bench test" or they are from "simulation" value?
I appreciate your kind support !!
Best Regards,