Part Number: ADS1232
Hi,
We are using ADS1232 for weighing scale application. With 10sps the output data is almost constant, but when we switch off the system and turn on again some times the output count what we are reading is wrong. When the system/ADC is working normally we read ADC count around 14800 but when the issue comes the ADC count what the controller reads is around 86400.
When the controller is powered on, we are pulling down the PWDN pin, after a delay of ~100ms the PWDN pin is made high for ~100ms and again pulled low for ~100ms and then the PWDN pin is made high and then the controller interrupts are enabled to read the ADC data when the DRDY pin is pulled low by ADC.
We would like to know what is causing the ADC to output wrong reading and how the issue can be solved.
Thanks,
Sreekanth