Hi,
I also have two questions about SNR measurement of AFE4404:
1) About receiver SNR, if this measure can be comparable with datasheet: applying a 0.5*FSR signal to input, calculate the STDEV of ADC data and calculate the SNR as: SNR=20*log10(2^22/stdev(ADC data)).
The datasheet specify SNR over 20Hz bandwidth, should a digital filter be applied to ADC data to limit the bandwidth to 20Hz before calculate the SNR?
2) How to measure the SNR of transmitter?
Thank you,
John